This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE5932: AFE5932-DESIGN的资源申请

Part Number: AFE5932
Other Parts Discussed in Thread: TX73L64,

 

My name is Zhanyan Li, and I am a master’s student at South China Normal University (Guangzhou, China). The university website is: https://www.scnu.edu.cn/.

I am currently working on the research and development of a miniaturized wearable ultrasound imaging device, targeting human vascular imaging and continuous blood pressure monitoring.

Please find the relevant project details below:

End equipment and application:
A wearable, miniaturized ultrasound imaging system for vascular imaging and continuous blood pressure monitoring.

Project timeline:
Prototype development is currently in progress. The project is focused on research and validation rather than immediate mass production.

Estimated yearly volume:
Low volume (research-stage project, non-commercial at this stage).

Company/Organization:
South China Normal University (academic research institution).

Transmit requirements:

  • Pulser levels: Bipolar (±100 V excitation)

  • Tx channels: 64 channels with beamforming capability

  • Desired output current: Moderate level suitable for driving PZT transducers (can be further specified if required)

  • Maximum excitation voltage: ±100 V

Receive requirements:

  • Rx channels: 64 channels

  • Signal frequency: Around 5 MHz ultrasound echo signals

  • Desired sampling frequency and noise: Suitable for 5 MHz imaging applications (low input-referred noise preferred; detailed specifications can be refined based on your recommendation)

  • Power per channel: Moderate, with consideration for wearable system constraints

Based on these requirements, I am planning to use the TX73L64 for transmission and the AFE5932 for reception as a combined solution for further system development.But my application was rejected.

 I would greatly appreciate it if you could provide driver code, software libraries, and any relevant development resources for these two devices to support my implementation.