请问TI大牛们,AFE4490正常工作时晶振是什么状态? 目前我的现象是:用微处理器通过SPI往AFE4490的某个寄存器写一个数据,也能正常读出寄存器的数据,数据也是正确的,但是测量晶振无反应, AFE4490的CLKOUT脚输出高电平。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问TI大牛们,AFE4490正常工作时晶振是什么状态? 目前我的现象是:用微处理器通过SPI往AFE4490的某个寄存器写一个数据,也能正常读出寄存器的数据,数据也是正确的,但是测量晶振无反应, AFE4490的CLKOUT脚输出高电平。
可能和晶振匹配电容有关,你选的晶振负载电容多大?匹配接的多大的?
20pF是晶振的负载电容还是电路中选择的匹配电容为20pF?
如果负载电容为20pF,那么匹配电容C1和C2的值一般选择在27~33pF之间。