Part Number: ADS1299
基本背景:ADS1299能够正常工作,根据手册和开发板参考设计进行设计,并且启用了BIAS功能。所有通道的差分负输入都连接到了SRB1,SRB1作为统一参考位点连接到右侧耳垂。BIAS输出电极连接到左侧耳垂。PGA增益都为24。正电源为2.5V负电源为-2.5V
问题1:所有通道正常连接并且和皮肤良好接触,由于ADS1299是直流耦合,观察采样原始数据可以发现,所有通道会在20min-30min逐渐饱和,饱和趋势一致最后接近-0.1875V(也有时候一起接近+0.1875),这种发生推着时间变化饱和的原因是什么,需要怎样修改?
问题2:假设一块ADS1299开启了BIAS_PD使能,并且选择了通道123作为BIASSENS+和-。当我只是连接通道1,2,3时候,其余45678悬空 。此时4,5,6,7,8通道映入大量工频,1,2,3通道正常采样。对于1-8通道全部连接额情况,发现只连接良好的1,2,3通道采样信号的信噪比不如1-8通道全连接的情况,理论上每一个通道都有独立的滤波,放大和adc电路,请问原因是什么?如何解决