使用的是标准YY0885,在输入阻抗一项,要求输入阻抗大于10M,测试过程是
1.在导联间输入5mV的正弦波信号,测量输出信号幅值
2.在输入端串入620k电阻和4.7nF并联的阻容网络,要求此时输入5mV信号,输出偏差不能超过步骤1结果的6%
现在的产品不满足这个要求,偏差在10%左右,这个应该从哪儿入手更改呢?
电路方案基本是参照ADS1298 demo板的设计进行的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
问题原本发在放大区,然后管理员告诉我放到数据转换器区会得到更多解答,现在怎么还没有人看啊?!
然后我放大区那边的帖子还被迫不及待的删掉了
1。可以把信号直接加在ADS1298 的输入端,不经过前面的RC网络。看是否是前面有衰减。
2。可以试一下ADS1298 的内部测试模式,看是否准确。