Other Parts Discussed in Thread: TMP112
各位大侠好:
请教关于TMP112的问题,电路中使用DCDC给TMP112供电,使用4.7K电阻和0.1uf电容给TMP112的供电管脚滤波,IIC总线的上拉电阻为4.7K,和FPGA管脚相连。
单独加载一个IIC模块读取TMP112的温度值正常,加载其他模块后随着电路功耗的增加,读取的温度值为全0和全1的概率增加,直到最后无法读出正确的温度值。
在此过程中使用示波器监控FPGA输出波形均正常,TMP112输出的波形异常。用示波器监控TMP112 的供电,在读写时,3.3V电源有100到200mV的波动(因有滤波电路),即使把滤波电路去掉,异常现象依然存在。
请问大家TMP112的供电有什么特别的?,是不是在读写数据前必须有什么初始化操作?