This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC7135发烫、发热

Other Parts Discussed in Thread: TLC7135

HI,TI:如上图设计,使用稳压电源供电接入+5V和-5V,开电后大约1分钟左右,TLC7135开始发烫,+5V的电流也从70mA(+5V也供电给MCU)变为230mA。请问我的设计是否合理?是什么原因导致这个问题呢?

  • 没给任何输入信号,测的静态电流都有这么大?

  • 是的,没有任何输入信号.我还特意见两输入端断接在一起,让输入信号为0V,问题的现象和两输入端的开路的现象一样:发烫.

    我怀疑是内部的放大器饱和了,但无法证实我的怀疑.这款芯的资料较少,DATASHEET介绍也较少,也没有参考设计电路,我实在无从下手解这个问题.

    给120kHz的时钟信号给芯片,BUSY脚是有输出方波的,同时,也发现有无120kHz的时钟信号给芯片,它都同样会发烫

    请问我该做什么实验来证实芯片是好的?定位芯片发烫的原因呢?