This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
拜见各位大神,小弟有如下疑问,还请帮忙,谢谢!!
1.若我采用8个ADS1259同时挂在SPI总线上然后至LPC1788,那么每个ADS1259的控制线(ADRST/RESET/DRDY/CS)应当如何接到LPC1788?求大神解答。
思路如下:
将CS1:CS8分别连接到LPC1788的IO脚,然后8个AD的ADRST连接在一起接到LPC1788的IO脚,8个DRDY连接在一起连接到1788的IO脚,8个RESET连在一起连接到1788的IO脚?是这个意思吧?
即8个AD的采样控制信号同步,即采样同步,然后LPC1788通过SPI总线读取哪一路由CS1~8来选择?
不知这样是否合适?
2.ADS1259可以不与PGA280一起使用吧?我在前端加其它的放大器,然后单端输出而非差分信号给ADS1259合适不合适?
3.如果我采用ADS1259的内部AD和内部VREF,和外部加晶振和外部参考电压有什么区别,是不是使用内部的内部AD和内部VREF,最后采样到的结果精度要差一些?
4.ADS1259采用+5V模拟电源和正负2.5V模拟电源供电时,对输入电压范围有没有影响?是不是我都可以输入电压为正负2.5V?
1.这些状态脚建议独立连接。
2.读取那一路可以由CS脚来选。
3.ADC可以接成伪差分的形式,输入单端信号。
4.内部REF方便,当系统中有几个ADC,DAC时,使用外部基准更方便校准。
5.是的。