现象描述如下:
1.ADS1278的供电5V、3.3V、1.8V输入正常
2.ADS1278晶振使用12MHZ
3.模式配置:MODE[1:0]:[1,0],选择低功耗模式
4.模式配置:FORMAT[2:0]:[0,0,1]选择SPI TDM模式 FIX模式
问题:处理器周期发出同步信号SYN,DRDY信号应该会有下降沿输出(数据准备好),现在DRDY一直维持高电平;但在处理器初始化后没有启动AD采集之前,即没有发出SYN负脉冲,DRDY却输出周期性正脉冲。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
多谢,经查DRDY功能正常了,但DOUT上读出的数据不正确,AD1278的SPI接口能否直接与F2812的SPI接口连接,即SCLK直接连,DOUT直连SPISOMI,DRDY接IO口进行查询,变为低时启动SPI发时钟读数据。但手册上介绍的与5509的MCBSP接口连接,DOUT需要接反相器和74门,对此不理解,其接SPI接口也需要这样吗?