This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1262输入信号是单端信号怎么连接?

Other Parts Discussed in Thread: INA333, ADS1262

想用1262做一个天平,但是桥的输出信号不够大,所以在桥和1262中间加了个ina333做放大,ina333的输出是单端信号,我的1262由5v单端供电,并且参考源选择供电源,输入信号通道为ain5做positive,ain6做negative,我将ain6接到ina333的地,ain5接ina333的输出端,在1262的GAIN=1时,得到的转换结果是对的,后调整GAIN=2,得到的转换结果只是GAIN=1时的1.2倍,并不是两倍,调整GAIN=4时得到的转换结果也只有1.6倍,所以我检查了我的电路连接方式。

首先去掉了ina333的放大电路,将桥的信号直接接入到1262,重新测试,得到的结果是正确的,随着GAIN的变化,转换结果也在成比例的变化。

其次,有了上面的测试结果后我基本明白了是因为1262的信号输入方式不同造成的,查找手册说可以使用aincom作为公共端,并且内部打开level shift作为查分信号的基准,可是问题是我的电路是单电源+5V供电的,输入的信号也没有2.5V大,那么我该怎么解决呢?我的信号参考地该怎么连接呢?