Other Parts Discussed in Thread: MSP430G2553, TLC1549
#include <msp430g2553.h>
#define uchar unsigned char
unsigned int mi=0;
double ni;
unsigned int adc(void)
{ unsigned int result=0;
int i;
P1OUT|=BIT1;
_delay_cycles(3);
P1OUT&=~BIT1;
for(i=0;i<10;i++)
{P1OUT&=~BIT2;
_delay_cycles(2);
result=((result<<1)+(P1IN&BIT3)/8);
_delay_cycles(1);
P1OUT|=BIT2;
_delay_cycles(4);
}
_delay_cycles(20);
P1OUT|=BIT1;
return (result);
}
void main(void)
{
WDTCTL = WDTPW +WDTHOLD; // Stop Watchdog Timer
P1DIR |= BIT1+BIT2;
while(1)
{
mi=adc();
ni=(mi)*(double)5/1024;
}
}
用TLC1549测稳压电压,怎么这个程序测得不准啊?而且值一直变,怎么回事啊?(BIT1是片选,BIT2是时钟,BIT3是数据输出)