在XTR115电路中,RSET电阻设置为3.375k,用的是精度0.1%电阻,当电压输入是2.7v时,电流输出8.2mA,电压输入为4.06v时,电流输出为12.36mA,转换精度为3%左右,但说明书给的转换精度很高,为0.015%,请问下是什么原因,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.