我使用的传感器为输出是差分信号,通过AD8221进行放大,之后经过一个电压跟随器给ADS1256;继电器不工作的时候,一切正常;每当继电器吸合或者断开都会让ADS1256复位;
继电器跟AD模块采用的是独立的开关电源,继电器是控制交流电磁阀;
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们公司ADC采集IC几乎都是ADS1256,一直都有这样的干扰现象,一直都没有解决,因为之前客户都是使用的固态继电器,就没出现过这样的问题;后面改为触点继电器就出现这样的问题,而且客户还不同意继续使用固态继电器,估计是成本原因;
今天我下午的时候,使用两块控制板,一块板只负责控制继电器(1S吸合一次),另一块板插上传感器;(这两块板完全没有任何的联系)大概工作6分钟,插传感器的那个控制板就出现复位的现象;用示波器观察,电压的波形很正常,没有明显的抖动;干扰应该是从传感器传导进来的,但是示波器又没有看到异常;
如果使用ADS1232就没有出现复位的现象,但是它的速度太低了只有80次;ADS1256出现复位的原因好奇怪,我初始化的时候是500HZ,当出现复位的时候,我有时候暂停0.2S不给ADS1256发送SCLK信号,就采集频率又能恢复到500;我检查过我的软件,没有发送过复位没有信号,也没有发送特定的SCLK时序给ADS1256;
这个问题困扰我好久了,一点办法都没有了;