This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS805的CM脚有什么用?

Other Parts Discussed in Thread: ADS805, ADS803

不太清楚ADS805的CM脚有什么用,而且对于使用手册上的说明没怎么看懂,请大神指点一下ADS805怎么使用,我按照手册在面包板上搭了个电路,我输入直流电压,显示的结果一直在跳而且幅度很大,不知道怎么回事,还是那个电路的问题,我是直接用跳线和MCU连接的,给ADS输入的频率为1.23Mhz,MCU主频为8Mhz .

  • 你先看手册图4,这幅图说明了CM脚的原理,其实就是在REFT和REFB之间接了两个800 Ohm电阻,把两个REF脚的中间值取出来。这个脚的用法在图3中有说明,比如你有一个单端信号,用交流耦合到变压器,那么传到变压器另一侧的电压就是直流为0的纯交流差分信号。但是805是一个+5V供电的ADC,不能直接处理+/-信号,所以需要把输入信号搬到一个直流上。图3的意思就是把CM注入到变压器中点,那么变压器另一侧的信号就是CM+input_AC,CM-input_AC,从而可以适应ADC的输入范围。

  • 如果一直在跳,建议先看一下是高位跳还是低位跳,如果是低位跳,看看是低几位在跳。然后检查一下电源,时钟,基准,CM是否给对;前端驱动能力是否足够驱动ADC。另外,TI有很多5M以下的ADC,14位,16位的都有,价格都比801便宜。你现在才跑1.23M的时钟,需要选801这么快的ADC吗?

  • 我设计的ADS803输出也一直跳  后来在淘宝买的ADS805模块  后来测试 还是一直跳  高低位都有跳变

    而且那个OVR引脚  怎么都不过载  

    调几天了 还是这样  实在不知道为什么?

    扣扣:1454988440  

    希望一起探讨