Other Parts Discussed in Thread: TL431, TLC2551, LM358
用TL431提供参考电压,后接LM358做射级跟随器来降低输出阻抗, 同时给两个TLC2551提供参考5V电压,结果电压被拉到3.8V,然后去掉一个AD,参考电压可以到5V,但是SDO没有数据输出,怎么办啊?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你的358,电源电压给的多少?从TINA仿真来看,5V的输入进去,电源电压要在6.5V以上才能保证输出跟随输入。会不会是电源电压给低了?
发上来的图打不开,没有装相应的软件,可否把电路图导出成.bmp或者.jpg文件再用附件发上来?
开始是给LM358一个5V的电压,后来见不对,又在板子上临时改成12V的了。射级跟随器能正常工作,但是AD不行!
那么改成12V电源电压以后,射级跟随器可以同时带起两个ADC的基准输入口了?如果基准没问题了,那描述一下AD的问题?所谓“不能正常工作”有哪些表现?先打个直流进去,看看输出对不对。
改成12V以后还是不能带两个AD,我把其中一个去掉了,这样参考电压对了,但是AD还是不能工作(SDO没有信号输出)。
对C语言不甚了解,不过从代码上看,你的~CS似乎只持续了16个SCLK,这是不对的。从手册上看,两个~CS之间至少要有44个SCLK,12个读数据,中间4个不用管,最后18个用来采样。你现在似乎只给了读数据的16个,中间间隔的4个和采样的18个SCLK都没给。