This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
单片机和ADS1118一直用5V电源,以32bit传输方式写入配置数据后,读到的寄存器返回值与写入的一致,但是读到的数据始终是0X7FF0,无论模拟输入端电压怎么变化都是这个值;
后来将单片机及ADS1118的电源改用3.3V,读到的数据就随着模拟端输入的变化而变化了,这是为什么??datasheet上给出的最大工作电压不是5.5V么??为什么5V系统不能正常工作?
没错, 手册强调了宽电压范围, 2- 5.5V 的工作范围.如果撇开 ADS1118 的问题, 那么还有是不是你的MCU 端的信号电平的兼容性问题呢?
MCU工作电压范围是1.8V~5.5V,实际使用中是与ADS1018接的同一个电源,同时接5V,或者3.3V的,
Nancy,
你的PGA[2:0]怎设置的,确认5V供电时输入没有超出满量程范围吗?
Sulyn Zhang