This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298 数据手册

Other Parts Discussed in Thread: ADS1298

尊进的工程师:
               我正在调试ADS1298,遇到了以下几个问题:
1、我按照数据手册上的时序进行了相应的初始化操作,如CONFIG1  0X06,, CONFIG2 0X13, CONFIG3 0XCCCH1SET0X10,CH2SET~CH8SET0X80,发送连续读取指令后我用示波器测得DRDY引脚上的电平频率为225Hz, 我把CONFIG1的值改为0X04,DRDY的频率跟着变为1k,这个我认为是正确的,但是我随后读取了所有的之前写入的寄存器,但是返回值都是0。。我不明白这是什么原因。
2、由于我只用到了第一通道,我就只采集了前6Byte数据,但是我打印出来发现,数据整体往后移了一个字节,如前三个字节表示status,应该是 11000000 00000000 00000000,但是实际上是 0000000011000000 00000000。我后来在第一次读取之前加了4 tclk 的延时,问题依旧。于是我人为的多读了一个字节的数据,然后从第二个字节开始取,然后用信号发生器产生方波(高电平2V,低电平0.5V,频率1Hz), 差分输入第一通道,波形正确,调整信号发生器的频率和幅度,采集后的波形也会相应变化,但是把信号换成正弦波以后,在顶部和底部不行都失真,并且整体上还是一个方波。
希望各位有经验的工程师给予解答