This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS805电路的数据采集问题

Other Parts Discussed in Thread: ADS805

ADS805电路是参照数据手册Fig5和Fig7设计的

采集电压范围0-5V,内部参考电压,采样频率20MHz

为测试电路的正确性,将Signal串1k电阻接GND,单片机采集的电压为0.3V

用万用表测各引脚的电压为:VCC=5.1V,Signal=0.3V,VREF=2.48V,REFT=3.72V,REFB=1.24V,CM=2.28V

请问,为什么会出现0.3V的偏差?

x 出现错误。请重试或与管理员联系。