Other Parts Discussed in Thread: AFE4404, ADS1291
我在用ADS1291和AFE4404组合做一个产品,在使用中遇到些问题:
第1:ADS1291中有个Offset Calibration的命令起什么作用?何时使用,是启动时校准一次还是要周期性地校准?
第2:AFE4404中有个Offset DAC配置指令,这个起什么作用? 如何使用?
项目挺赶地,盼各位专家给我快速解答一下,不胜感激!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
看看手册的说明
OFFSETCAL: Channel Offset Calibration
This command is used to cancel the channel offset. The CALIB_ON bit in the RESP2 register must be set to '1' before issuing this command. OFFSETCAL must be executed every time there is a change in the PGA gain settings.