各位工程师:
您们好!TLC5615是一款DA芯片,我原来用的是2.5作为其的参考电压,突然转为2.048作为参考电压,会使芯片报废吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位工程师:
您们好!TLC5615是一款DA芯片,我原来用的是2.5作为其的参考电压,突然转为2.048作为参考电压,会使芯片报废吗?
你好 Zhou,
TLC5615这颗芯片参考输入端口的电压,可以正常进行数据转换操作的为小于AVDD-2V(AVDD即为电源电压);另外,保证芯片不损坏的电压范围为-0.3V到AVDD+0.3V之间,所以你参考接2.048不会使芯片报废。但是相同码值,转换出来的电压值会等比例缩小
Best regards,
Sulyn Zhang
TI工程师,您好,谢谢您的回答。如果供电电压5V,参考电压是2.5V,那会不会影响TLC5615工作?
您好,谢谢您的回答,我程序中没有用到对DA的寄存器操作。还请问这个寄存器操作该怎么操作?