Other Parts Discussed in Thread: ADC08D1520
我在使用Xilinx FPGA V5 对ADC08D1520进行配置的时候出现了这样的问题,使用Extended Control Mode对ADC的寄存器进行配置,但是ADC的DCLK始终没有输出,一直输出50mVpp左右的噪声。
我使用ADF4355锁相环为ADC08D1520提供500M采样时钟,当只配置ADF4355而不配置ADC08D1520时,ADC的输出DCLK为共模电压150mV,Vpp=50mV左右的噪声,而当我对ADF4355和ADC08D1520都进行配置时,输出的DCLK为共模电压270mV,Vpp=50mV左右的噪声,所以我不清楚我是否对ADC08D1520的寄存器进行了操作。
我按照ADF08D1520的技术文档对9个只读寄存器进行了配置,SCS,SDATA和SCLK的时序都满足要求,不知道这颗芯片的配置还需要哪些应该注意的地方,请各位大神帮忙解答一下,谢谢