This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE5808的数字输出输入电压问题

Other Parts Discussed in Thread: AFE5808, AFE5805

数据手册上,AFE5808的数字供电DVDD是1.8V,但其数字输入高电平VIH却是2-3.3V,很奇怪,是不是数据手册错误?

而且数字输出高电平最大是DVDD,也就是SPI配置AFE5808时,输入SCLK,SDATA,SEN和输出SDOUT电平是不一样?

AFE5805的DVDD是3.3V,其数字输入高电平VIH是1.4-3.3V,一比较,AFE5808很奇怪。

  • AFE5808的Vih, Vil看起来确实让人迷惑 ,DVDD只是AFE5808 的ADC数字部分供电电压,

    这里的Vih和Vil参考的应该是AVDD,也就是说除了ADC数字部分,其他数字IO的Vih,Vil电压。 datasheet中Absolute maximum rating中:

    Voltage at analog inputs and digital inputs:  –0.3V~ [3.6, AVDD + 0.3]V

  • 手册里,DVDD: ADC digital and I/O power supply, 1.8 V,应该包含数字IO,比如SPI 。

    按照数据手册,与spi连接的单片机或fpga应该用什么电源电压?用1.8?还是3.3?还是1.8与3.3共用?