This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1210 应用问题

Other Parts Discussed in Thread: TUSB1210

Dear All ,

我有个关于TUSB1210的问题。

1》TUSB1210这块IC,我们需要用STM32F103配置并口传输达到高速USB传输(实际需要5M/S以上的传输速率)。您这块IC是否电脑端免驱,我们的并口配置方面是否直接按照8bit字节读写即可转为USB。如果有注意事项,请告知。

2》达到高速USB配置时,我们的单片机方面的几个接口(STP、NXT、DIR、CLKIN、REFCLK)的信号控制方式。

3》该IC有多个模式可供选择,并通过memory进行配置,建议提供采取不同模式的配置方案的实用后的固件或文档。

  • 这是个 USB2.0 高速 480Mbps ULPI PHY 收发器,  实际需要5M/S以上的传输速率是可以实现的. 倒是你的 MCU 端怎么提供这个速率还有待验证.

    至于是否免驱动, 还得看系统, 这个芯片已经出来比较久了, 新的系统能够內带这个驱动了吧