This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE4400问题

Other Parts Discussed in Thread: AFE4400

1、  术手册中有关ADC采样频率的说明,在第10页中说采样率为4*PRF

而在第40页中关于ADC Data的中可以采样率为16*PRF

但是如果我将占空设置为25%以下时,采样率又该如何计算?

2、  我在测试中发现,改变LED发光时间长度和对应的采样时间长度,采集到的原始波形是不相同的,发光时间越短波形只有一个峰,

发光时间达到一定长度时,就会出现两个波峰,这种现象如何解释,其他条件都一样,如下图中是有两个波峰的

3、  在计算血氧值时,会出现计算不准的问题,我们的算法是没有问题的,之前使用的运放搭建的电路,精度较高

  • PRF 是可以调节的

    In cases where the device is operated with low pulse repetition frequency (PRF) or low LED pulse durations, the active portion of the pulse repetition period can be reduced. Using the dynamic power-down feature, the overall power consumption can be significantly reduced.

  • 1. ADC实际转换一次的时间是50us,即200个CLK。AFE4400会对每个通道的信号连续进行3次转换并取平均的到转换结果,所以,无论占空比如何,PRF如何,只需给每个通道留够600个CLK的时间就行。当然,还要多留些时间以便采-保电路稳定。

    2. 如果时序设计不合理是会导致错误的采样结果的。

    3. 同2.