This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求教:适合与DAC7811匹配的运算放大器,DAC7811的带宽问题

Other Parts Discussed in Thread: DAC7811, OPA277, OPA227, OPA177, OPA228, OPA657, OPA698

我按照DAC7811技术手册的Figure 26焊了个程控衰减器,对5Vpp的正弦交流信号进行衰减。但是一直没有找到匹配的合适型号的运算放大器。

信号的频率范围是1K~10MHz。

我试过OPA227、OPA277、OPA177。均因为压摆率不足而在小于500KHz时就失真了。

我还试过OPA228、OPA657。结果因为不明原因,输出的波形带有高频率的、幅值大于1Vpp的谐波。可见运放的选择也是有要求的。

效果最好的是OPA698,在1.6MHz以前波形良好,幅值调节的线性度也很高。但是之后继续增加频率,就发生了类似谐振的现象(也有可能就是谐振),在固定衰减倍数为1的时候,输出幅值随频率增大而增加,在8MHz左右达到峰值,增益将近2倍。而后幅值减小,在10MHz时增益为0.8~0.9。

芯片手册上写的10MHz乘法带宽,所以应该有合适的运放可以让衰减器的带宽拓展。

求问:技术手册 Figure 26 中的运放选择有什么要求?可否推荐合适的运放以使该衰减器的带宽增加(最好可以达到理论的10MHz)?