This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1210+AMC1203的疑问

Other Parts Discussed in Thread: AMC1210, AMC1203

你好。

我使用1颗AMC1210+3颗AMC1203,进行永磁同步电机的反电动势采样,现在能够从AMC1210的数据中获得波形,但是我的疑问是:

AMC1203的输出是一个PWM的占空比信号,+280mV时输出87.5%的占空比,-280mV时输出12.5%的占空比。

AMC1210的输出与之对应的关系是什么?例如我使用sinc3,256次过采样,然后数据移位SH设置为9,这样得到的-32767到32767的结果,与AMC1203的PWM的映射关系是什么?

是0%对应-32767,100%对应32767?

谢谢。