This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1282HIPW和ADS1282IPW有什么区别?

Other Parts Discussed in Thread: ADS1282

ADS1282HIPW和ADS1282IPW有什么区别?

  • H是高性能的意思

    The H version of the ADS1282 has an improved input stage compared to the base version ADS1282. The ADS1282H design is optimized for use with high
    impedance sensors, such as hydrophones. The ADS1282H is recommended when interfacing to hydrophone sensors and can also be used for low-
    impedance, geophone sensors as well. The base version ADS1282 should only be used with low-impedance geophone sensors, where the associated external terminating resistance is < 50kΩ (per resistor).

  • 楼上的说明,在哪找到的呢?