This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8568 问题

Other Parts Discussed in Thread: ADS8568

我用fpga 控制ADS8568,具体设置如下,当输入25khz 4V 正弦信号时,量化值为15904,远小于26213,但是输入25khz 2V 或者2V以下时,量化值正确,这是什么原因?我测试了下VEFIO,值为4.8V,是不是这个原因?该怎么改? (程序的采样率为200k,AD参考电压选择默认2.5V)

HW/SW =0,

REFEN=1,

RANGE=1,

HVSS = -5.2V, HVDD=4.6V(实测值)

  • 前端放大器是何型号,检查滤波器截至频率是否满足要求。

    此外请检查转换速率是否在参数要求范围之内,串行接口最快转换速率为400ksps。

    前端放大器选型和转换速率之间会有一些要求,请查看相关应用笔记。https://training.ti.com/engineer-it-how-select-op-amp-drive-your-sar-adc?keyMatch=SAR OPAMP&tisearch=Search-EN-Everything

  • 您好 Hawk  Tong:

            我之前前端放大器用的是ADA4841-2,现在改成了OP284,测试给到AD的信号没问题。现在VEFIO正常情况下应该2.5V,而我的是4.8V,这是什么原因?我已经更换了AD。电路原理图如下: