Other Parts Discussed in Thread: ADS8361
能不能给菜鸟推荐下16位4通道 运行稳定的AD 谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电源电压,输入信号的频率/共模/摆幅,基准,输出是用SPI还是用I2C,把信息给的全一些。
频率不怎么要求 500K就足够了 协议用SPI吧 基准5V
推荐ADS8361,16bit,500KSPS,串行SPI接口。支持单端信号和差分信号。内部基准2.5V,Full scale可以达到5V。
到这个链接下,选一下就ok了