This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA900能够输出4-20mA的同时,外部MCU能够通过SPI读取ADC寄存器的测量值吗?

Other Parts Discussed in Thread: PGA900

我想使用PGA900开发压力变送器,输出4-20mA信号,同时变送器本体加一块液晶显示屏实时显示测量值,显示功能通过另外增加一个MCU通过SPI读取PGA900内部的ADC值实现,我想知道PGA900在保证不间断输出4-20mA模拟量信号的同时,还能够实现通过SPI通讯吗?

  • 此处假设你会用到两线制4-20mA输出,功耗会是关键问题之一。PGA900的静态电流大约在2.2-2.5mA范围,如果考虑前端压力芯体激励电流0.5mA,功耗基本可以满足前端需求。需要提醒一句,PGA900的通信接口SPI/I2C只能作为从模式应用。