This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于TLC5510采样频率的问题

Other Parts Discussed in Thread: TLC5510

TLC5510模数转换芯片,如果我需要转换10M的信号,那么芯片的采样时钟频率则至少需要20M,或者更大,单片机无法产生这么高的时钟频率,我该如何得到高频率的时钟信号呢

  • 如果你需要转换10M带宽的信号,用20M的采样率是不可以的。虽然能满足乃奎斯特采样定理,但不推荐这样做。建议用2.5倍以上的频率进行采样。

  • 如果需要的时钟速率比较高的话,可以采用专门的时钟生成芯片。比如高端的LMK04XXX系列,终端的LMK03XXX,低端的6100X系列

  • 1. 如果你的信号是个低通10M信号,就是说,频率成分从低频段一直到10M都有,那建议你换一个采样率更高的ADC,因为TLC5510最高只能支持到20MHz的采样率。如果你的信号是个带通窄带信号,就是说,信号成分集中在10MHz附近的窄带里,那可以考虑用个较低的采样率去采,比如9M~11M的信号,你用12M的时钟采,最后混叠到低频段也就是1M~3M。

    2. 你要只是用到8位就够了,那买个质量一般的晶振就行,没必要用LMK系列的时钟。LMK04系列,官网报价比你5510还贵,你用的时候还得外挂一个晶振,不值。

  • 学习了第一条信息。支持一个。