This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助,DAC8760输出4-20ma不对!

Other Parts Discussed in Thread: DAC8760, DAC8750

一直在调DAC8760,输出范围4-20mA, 目前发现只能输出0mA 和 24mA,不知道什么原因,我附上程序,请帮我看看,是不是我配置的问题?






//库文件名: dac8760.h 
#ifndef _dac8760_H 
#define _dac8760_H   
//*********************************************************** 
//以下是使用到的SPI通讯端口,需要根据实际连接情况进行配置 
#define DAC8760_GPIO                 GPIOB  


#define DAC8760_DIN_GPIO                 GPIOD 


#define DAC8760_DIN                         GPIO_Pin_2 
//写数据线 
#define DAC8760_SCK                         GPIO_Pin_3 
//时钟线 
#define DAC8760_LAT                         GPIO_Pin_4 
//使能线   
#define DIN_1                                         GPIO_SetBits(DAC8760_DIN_GPIO, DAC8760_DIN)   
#define DIN_0                                         GPIO_ResetBits(DAC8760_DIN_GPIO, DAC8760_DIN)  

#define SCK_1                                         GPIO_SetBits(DAC8760_GPIO, DAC8760_SCK)   
#define SCK_0                                         GPIO_ResetBits(DAC8760_GPIO, DAC8760_SCK)  
                                                      
#define LAT_1                                         GPIO_SetBits(DAC8760_GPIO, DAC8760_LAT)   
#define LAT_0                                         GPIO_ResetBits(DAC8760_GPIO, DAC8760_LAT)    


//********************************************************** 
#define V_0_5                                          0x0000 
//电压范围0-5V 


#define V_0_10                                         0x0001 
//电压范围0-10V   


#define I_4_20                                         ((unsigned short)(1<<9)) 
//电流范围4-20mA 


#define I_0_20                                         ((unsigned short)(2<<9)) 
//电流范围0-20mA 


#define I_0_24                                         ((unsigned short)(3<<9)) 
//电流范围0-24mA   
//**********************************************************


extern void DAC8760_Init(void); 
extern void DAC8760_Out(unsigned short dat);  
#endif




//文件名: dac8760.c  
/****************************************************************************
                                                                                           DAC8760控制程序  
****************************************************************************/
#include "common.h"


//********************************************************** 
void DAC8760_Write(unsigned char add,unsigned short dat); 
void DAC8760_Config(void); 
void DAC8760_Init(void); 
void DAC8760_Out(unsigned short dat);


void delay_ms(unsigned int cnt)
{
        unsigned int i;


        for(i = 0; i < cnt; i++)
        {
         __nop();
        }
}


//写寄存器 
void DAC8760_Write(unsigned char add,unsigned short dat)
{  
        unsigned char i;   unsigned char h_8bit, l_8bit;     
        h_8bit=(dat>>8)&0x00FF;
        //取高8位数据     
        l_8bit=dat&0x00FF;     
        //取低8位数据   
        LAT_0;    
        for(i=8;i>0;i--)//写8位地址
        {    
                SCK_0;    
                if(add&0x80)   
                {    
                        DIN_1;    
                }   
                else   
                {    
                        DIN_0;    
                }     
                delay_ms(100);
                SCK_1;       
                add<<=1;   
        }


        for(i=8;i>0;i--)
        //写高8位数据  
        {    
                SCK_0;     
                if(h_8bit&0x80)   
                {    
                        DIN_1;    
                }   
                else   
                {    
                        DIN_0;   
                }      
                delay_ms(100);
                SCK_1;       
                h_8bit<<=1;     
        } 


        for(i=8;i>0;i--)
        //写低8位数据  
        {    
                SCK_0;     
                if(l_8bit&0x80)   
                {    
                        DIN_1;    
                }   
                else   
                {    
                        DIN_0;   
                }      
                delay_ms(100);
                SCK_1;       
                l_8bit<<=1;    
        }    
        delay_ms(100);
        LAT_1;  
        DIN_1;
}


void DAC8760_Config(void) 
{  
        DAC8760_Write(0x56,0x0001);  
        delay_ms(1000);        
        //复位所有寄存器;   
        DAC8760_Write(0x55,(1<<12)| V_0_5); 
        delay_ms(1000);
        //控制寄存器设置;    DB12 输出使能   | 电压输出范围0-5V  
        DAC8760_Write(0x57,(1<<8) | I_4_20); 
        delay_ms(1000);
        //配置寄存器设置;    DB8  双输出使能 | 电流输出范围4-20mA     
        DAC8760_Write(0x01,0); 
        delay_ms(1000);
        
        //输出0  
}


void DAC8760_Init(void)
{   
GPIO_InitTypeDef GPIO_InitStructure;
  /* Configure  DAC8760  */
  GPIO_InitStructure.GPIO_Pin   = GPIO_Pin_3 | GPIO_Pin_4;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
  GPIO_InitStructure.GPIO_Mode  =  GPIO_Mode_Out_PP; 
  GPIO_Init(GPIOB, &GPIO_InitStructure);        

  GPIO_InitStructure.GPIO_Pin   = GPIO_Pin_2;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
  GPIO_InitStructure.GPIO_Mode  =  GPIO_Mode_Out_PP; 
  GPIO_Init(GPIOD, &GPIO_InitStructure);        





        DAC8760_Config();
}   


void DAC8760_Out(unsigned short dat) 
{  
        DAC8760_Write(0x01,dat);