波形幅度在0到5V时每个波形的零点有一个点的飞点直接上升到电源点5V。当再调大输入波形大于5V时在波形的每个5V点也产生飞点到10V。我的输入波形经过1/4分压量程10V,参考电压是2.5V。问题的原因搞不懂请赐教。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
手册25页图67画出了输入级的等效电路,从这个电路看,开关在打开和关断时会向两端泄放电荷,从而造成一些尖刺。如果泄放的电荷过多,有可能把保护二极管冲开,以至于尖刺直接冲到VDD/GND。建议参考38页图88,在输入端加入一个电容,在不影响前级驱动能力的情况下,加大这个电容有助于吸收泄放的电荷。
如果交流信号输入时有尖峰,建议你计算一下尖峰的频率,看看是否和信号的频率有相关性。另外,看一下尖峰出现在哪个输入电压下,从你第一幅图来看,尖峰总是出现在0V,但是第二幅图尖峰对应的输入电压又变化了。
1. 上传一下你的电路图,最好能把ADC的前端信号调理电路也一并传上来。
2. 从手册24页表格5来看,VINP-VINN=0时对应的是0;VINP-VINN~=-VREF时对应的是800000h。你的结果不对吧?
fclk是跑在32.768M下吧?这个时钟在32.768M以上时,基准要给到2.048V的。
按照手册25页图71再确认一下,REFP驱动能力够不够。
还有就是VCOM和VCOM1.从电路图上看,这两个节点现在应该是用0欧姆电阻短路的,如果把R5去掉,情况是否有改善?