This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

12bit 8通道DAC选型

Other Parts Discussed in Thread: DAC8564

你好,请问:

        TI对标ADI的AD5672这款DAC的物料(性能相近也可)?

谢谢!

AD5672简介:

AD5672R/AD5676R分别是低功耗、8通道、12/16位缓冲电压输出数模转换器(DAC), 内置2.5 V、2 ppm/˚C内部基准电压源(默认使能)和增益选择引脚,满量程输出为2.5 V(增益=1)或5 V(增益=2)。 采用2.7 V至5.5 V单电源供电,通过设计保证单调性。 这些器件采用20引脚TSSOP封装。

AD5672R/AD5676R还内置一个上电复位电路和一个RSTSEL引脚,确保DAC输出上电至零电平或中间电平,直到执行一次有效的写操作为止。 每个器件都具有各通道独立掉电特性,在掉电模式下,器件功耗降至2.5 µA。

AD5672R/AD5676R采用多功能串行外设接口(SPI),时钟速率最高达50 MHz,并均包含一个为1.8 V/3 V/5 V逻辑电平准备的VLOGIC引脚。

产品特色

  1. 高相对精度(INL)。 
    AD5672R(12位): ±0.1 LSB(最大值)
    AD5676R(16位): ±3 LSB(最大值)
  2. 低漂移2.5 V片内基准电压源