各位前辈,最近遇到一个数据采集的问题:1、首先采用PGA281可编程运放对小信号进行放大,但由于PGA281输出的是差分信号,因此如何对差分信号进行有源滤波呢?难道要在+、-两路上分别滤波吗?2、采集部分AD与FPGA之间的通信接口也是差分信号,参考TI数据采集解决方案,准备将AD与FPGA之间的差分通信线也进行隔离,现在就是没找到隔离差分信号的器件,难道要将差分信号单端化后在隔离?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
好像除了几款专门隔离CAN和485的收发器之外,目前的TI数字信号隔离器还没有隔离差分信号的。
模拟部分滤波,可以使用全差分放大器设计,像THS4551一类的,AD和FPGA之间如果要隔离,可以使用数字隔离器,像ISO7340一类的。