Other Parts Discussed in Thread: ADS1246
你好,最近在使用5418a连接6个ad1246,顺序进行SYS0 寄存器配置时设置采样频率20HZ(写入0x02),之后想测试配置是否成功(同时验证SPI口的通讯配置),对SYS0 寄存器进行读操作,发现读出来的数据不对,写、读操作分别为
ADC1_WDATA[0]=0x02; //Write SYS0 REG By 0x02; Data Rate =20 SPS
EXCHANGE_UCB0(0x40|0x03); //写寄存器:发送第一个地址字节(address = 03h)
EXCHANGE_UCB0( 0x00); //写的长度-1后的值(发送第二个字节)
EXCHANGE_UCB0( ADC1_WDATA[0]);
__delay_cycles( 20 );
EXCHANGE_UCB0(0x20|0x03); //读寄存器:发送第一个地址字节(address = 03h)
EXCHANGE_UCB0( 0x00); //Read REG
_NOP();
ADC1_RDATA[0]=EXCHANGE_UCB0( 0xFF);
__delay_cycles( 20 );
UCBORXBUF中读出来的分别是FF,7F,FF,7F,00,7F,理想的数据应该是0x02,不知道问题出在哪??
还有__delay_cycles( 20 )中延时的20个时钟周期对应的是主系统时钟MCLK,还是对SPI口配置的时钟信号(即对SMCLK分频后的时钟信号)??