Other Parts Discussed in Thread: ADS8528, ADS8568, ADS8548
各位好,我在选型使用ADS8528同步采集16路信号,每路采样率要求均达到140KSPS/12bit,输出数据与DSP连接,考虑使用2片ADS8528。
问题如下:
1、ADS8528的8路都能同时达到650KSPS采样率,还是单路使用时才能达到;
2、若8路能同时做到650KSPS,那么数据率就是650KSPS*8,而我在手册中看到的参数对于Throughput rate的描述,Serial interface, all four SDOx active是480KSPS,Parallel interface是650KSPS,我的理解是这个芯片总的数据传输率最大是650KSPS,那么8路同时达到650KSPS采样就没有意义了,不知道是不是这样理解;
3、我的DSP目前只支持1个24bit的EPPI和2个SPI,现在DSP和ADC都处在选型阶段,ADC主要应用是同步采集16路模拟信号(±5V,电平我也可以调整不作为限制),≥12bit,每路采样率均达到140KSPS,每路独立不要切换,现在主要限制在了DSP与ADC的数据接口上,现有的DSP能否实现,或者推荐一个DSP和ADC,谢谢!