想问一下,目前5个采集通道,用了5片ADS1675,不想各自干扰,数据线和时钟是差分的,这些控制线还有数据线都要隔离吗?如果做隔离,选择什么芯片好?还有可不可以只隔离控制线部分,上面几对差分对不进行隔离?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
想问一下,目前5个采集通道,用了5片ADS1675,不想各自干扰,数据线和时钟是差分的,这些控制线还有数据线都要隔离吗?如果做隔离,选择什么芯片好?还有可不可以只隔离控制线部分,上面几对差分对不进行隔离?
不需要加隔离芯片吧,控制线是数字信号, 但需要将模拟信号和数字信号分开防止干扰,模拟信号参考模拟地,数字信号参考数字地。
如果每片都加上隔离芯片,那板子的空间也势必会增大很多。
另外,如果需要5个通道的,可以直接选择多通道的ADC芯片,减少设计也减少板子空间,相对要方便许多。
你好,现在ADC选用是ADS1675,不想通道自己各自影响,而且我每个通道都是隔离电源,每一个通道都有一个,就是想把控制线进行隔离,不然给每个通道选隔离电源没有啥作用。控制线是8根,选两个4通道隔离芯片进行隔离,就是差分数据输出那3对,这里需不需要做隔离?
你好,目前我已经把控制信号都用ADuM240D隔离了,唯独每个ADC的差分对没有隔离,差分对速度太高,没有选到合适隔离芯片,能否推荐一个,不在乎价格。
还有一件事,如果隔离一个信号,用隔离芯片,是不是隔离芯片的最大频率要大于信号频率3倍以上?第一次用隔离,有许多问题,请赐教。