Other Parts Discussed in Thread: ADS1256, ADS1255
大家好,我在使用ADS1256做电压采样的时候,使用的单极采样,采集AIN0和AIN1两个通道的数据。在一个通道接入3.3V,另一个通道没有接入电压,采集到的数据AIN0通道电压达不到3.3,并且小的那部分会在AIN1通道获取到,但是我两个通道都接上3.3V后,两个通道采集的数据都正常,请问这是什么原因引起的呢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您的意思是采用单端输入,那么AINCOM怎么连接的呢?需要注意如果单端输入,不用的一端可直接悬空,但是AINCOM不能直接接GND,可以接1/2Vcc.
请问各位专家,ADS1256单端输入采样时,只用4个通道,其余的通道能不能悬空?另外,AINCOM到底是应该接地还是可接参考电压?我在采集时,用30Ksps对四通道采样,会偶尔相邻通道间的值会串,如通道1采2.5V,通道2采0.0V,通道3采3.3V,有时会在通道1输出3.3V,通道2出2.5V等。而且,测试较长时间采集(40min)时,采集的都不对?这可能是什么原因导致的。
在datasheet page14有对单端输入的介绍:
When using ADS1255/6 for single-ended measurements, it is important to note that common input AINCOM does not need to be tied to ground. For example, AINCOM can be tied to a midpoint reference such as +2.5V or even AVDD.
对于不用的输入端,可直接悬空:Leave any unused analog inputs floating. This minimizes the input leakage current
1.不用的通道输入可悬空,这个说法是只针对单端输入测量,还是只针对差分输入测量的?还是这两种模式下不用的通道都是可直接悬空的?
2.你说“需要注意如果单端输入...但是AINCOM不能直接接GND,可以接1/2Vcc.” 但,为何我看官方数据手册里面的Figure 25的推荐电路,AINCOM却是直接接地的,这不是自相矛盾吗?在网上流行的电路,甚至是某宝大量的成熟的ADS1256的模块,AINCOM都是直接接地的,而芯片数据手册写的是When using ADS1255/6 for single-ended measurements, it is important to note that common input AINCOM does not need to be tied to ground. For example, AINCOM can be tied to a midpoint reference such as +2.5V or even AVDD. 原版说法是does not need to ,意思是can't 吗?直接接了AGND会有什么后果?难道AGND不是ground?
3.AINCOM这个引脚实际是有什么作用的?
4.对于差分输入,不使用AINCOM,这个“不使用”的意思是在硬件连接的角度是指接一个固定电平?还是指悬空?还是指接不接都可以?如果是指悬空,我要在电路板上兼容单端和差分测量,然后接了1/2VDD,当我使用差分时,会不会是芯片工作不正常或者损坏芯片?