在做一个改版项目,之前用的8位LVT245 供电是3.3V的,发现输出信号幅度低于2.0V,现在想找一款供电兼容3.3V和5.0V的buffer,不知道有没有?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在做一个改版项目,之前用的8位LVT245 供电是3.3V的,发现输出信号幅度低于2.0V,现在想找一款供电兼容3.3V和5.0V的buffer,不知道有没有?
可以参考下SN74AHC245。供电电压范围为2V~5.5V。
另外,您提到的LVT245,如果是3.3V供电的话,Voh也不可能低于2V啊。但是如果您需要5V CMOS输入的话,这款不建议,因为这款是3.3V供电,但是兼容5V TTL输入,因为5V TTL和3.3V LVTTL门限电平一致。
查阅LVT245datasheet,Io=35mA,我信号的负载阻抗50Ω,Voh=35mA*50Ω=1.75V<2.0V