Other Parts Discussed in Thread: DAC8760, ADS1256
想做一个采集设备,采集信号为4-20mA,1到5V DC ,0-10VDC ,三种信号,要求精度不低于0.1%,刷新率为 25ms。在做一个输出 4-20mA,1到5V DC ,0-10VDC ,请问选用什么样的ADC 和DAC合适?ADC类型是选用 SAR 还是Sigma-Delta 。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您的意思是想选一款采集信号为4-20mA,1到5V DC ,0-10VDC 的ADC,还需要一款4-20mA,1到5V DC ,0-10VDC输出的DAC?
DAC的话您可以参考DAC8760,可以是4~20mA 电流输出,也可以是0~5V或0~10V电压输出。