请问如果采用电阻模式,只是改变连接方式么,如果是的话,我把它作为LDO中一个电阻,接的是WA和HA,LA悬空,但为何测出来WA电压为0,HA和LA电压都是高电压,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kai,
你好!这个电路在原理上是没有问题的,但是TPS7A8001的输出电压值与R2及RHW成比例关系,当R2固定为10K时,RHW按要求应该在0ohm至52.3Kohm之间变化以得到相应的电压输出。TPL0102-100内部集成了非易失性EEPROM来存储通过I2C总线所设定的电阻值,其最大值是100Kohm,建议你在使能TPS7A8001之前先通过I2C指令设定TPL0102的输出值,并读取验证,以确保得到你所需要的输出电压,谢谢!
Kai,
你好!请先确定TPL0102和TPS7A8001这两部分电路是共电源共地的,仍有问题的话则建议将电位器和LDO断开,单独测测电位器TPL0102工作是否正常:比如上电后RWH之间的电阻值是多少?通过I2C命令改写wiper的位置是否能正确改变RWH的阻值?等等。或者也可以通过TI的授权代理商申请TPL0102的评估板进行测试。更多问题,请联系Jenny-Jiang@ti.com, 谢谢!