我用ADS1256采集0-5V信号,PGA=1 ,关缓冲。参考电压设定为2.5V(精密基准源),采集AIN0的值,当AINP1和AIN1 短接时,输出1.018mV电压,AINP1和AIN1 电压为2.5016V,时输出2.4988V,相差2.8mV,AINP1和AIN1 电压为4.9984V,时输出4.9916V,相差7mV.误差很大,是怎么回事啊?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.