詢問TI人員
當THS1209 BVDD接到3.3V時,其輸出並列總線電壓為3.3V
但當DVDD接到5V時,會影響到這3.3V的系統嗎?
例如: SYNC(DATA_AV) Pin 會輸出5V還是3.3V ?
會這樣認為的原因是THS1206 DVDD是可接3.3V的,而THS1209只能接5V..
因我後端系統為DSP 3.3V,不知道是否會有哪些腳位受影響
板子即將送洗,還請解惑
感謝!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
THS1209的DVDD之能接5V,不能接3.3V。但是BVDD的范围为3V~5.25V.也就是说既可以是3.3V也可以是5V。
BVDD是给buffer供电的,如果3.3V BVDD,是不影响5V DVDD的。
SYNC不是buffer的输出,可以参考THS1209内部框图,所以输出是按照DVDD的输出结果,为5V的。