This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADS8422输入的差分信号的疑问,期待您的回复,谢谢

Other Parts Discussed in Thread: THS4131, ADS8422

TI团队你好!

我在使用THS4131驱动ADS8422,现有问题如下:

1、ADS8422的输入的两支差分信号都应该>0V,对吗?

2、前提:THS4131的Vcom=Vref/2;

      ADS8422手册中有讲full-scale电压范围是[-Vref,+Vref],两支差分信号的absolute电压范围也应该满足[-0.2,Vref+0.2],那么问题就是:按照full-scale范围算         输出的两支电压信号范围应该是[0,Vref/2];从差分信号的absolute范围角度看,如果两支信号的幅值都达到了Vref,

       那么(+IN)-(-IN)=2Vref(max),这显然跟full-scale范围不相符合啊?

3、如果ADS8422使用外部参考电压Vref=4.096V,那么其PIN3:COMMOUT会输出Vref/2=2.048V对吗?

4、(THS4131使用单端信号转差分输出工作模式,Vcom=Vref/2);对THS4131的单端输入信号来说,其信号峰值应该 <=4Vpp(ADC的Vref=4.096),因为如果峰值达到了8Vpp,那么两支差分信号的峰值就会是4Vpp,两者相减,就不满足full-scale电压范围是[-Vref,+Vref],而变成[-2Vref,+2Vref]了,对吗?

5、我大概知道了THS431的Vcom脚的作用是为了抬高输出差分信号的共模电平,目的是使其差分信号都大于0。我还是想请教一下官方对Vcom的解释。

  • 1.差分信号的输入范围没有限制必须是正的电压值的。

    2.你这么计算是错误的,只要保证(+IN)和(-IN)的范围不超过VCC,并且full-scale电压范围是[-Vref,+Vref]就是合理的。你那么算,是错误的,涉及到区间范围的扩大和缩小的问题。

  • 1、adc手册里讲了+IN和-IN的输入范围是[-0.2,Vref],那不就是说两支的差分输入得要大于0吗?

    2、如果我用4M采样率的adcADS8422对50khz的正弦波采样,对50khz的正弦波采样100个周期,需要多长时间?

    3、adc手册里写的最大转换时间是180ns,这个180ns该怎么理解呢?