Other Parts Discussed in Thread: THS4131, ADS8422
TI团队你好!
我在使用THS4131驱动ADS8422,现有问题如下:
1、ADS8422的输入的两支差分信号都应该>0V,对吗?
2、前提:THS4131的Vcom=Vref/2;
ADS8422手册中有讲full-scale电压范围是[-Vref,+Vref],两支差分信号的absolute电压范围也应该满足[-0.2,Vref+0.2],那么问题就是:按照full-scale范围算 输出的两支电压信号范围应该是[0,Vref/2];从差分信号的absolute范围角度看,如果两支信号的幅值都达到了Vref,
那么(+IN)-(-IN)=2Vref(max),这显然跟full-scale范围不相符合啊?
3、如果ADS8422使用外部参考电压Vref=4.096V,那么其PIN3:COMMOUT会输出Vref/2=2.048V对吗?
4、(THS4131使用单端信号转差分输出工作模式,Vcom=Vref/2);对THS4131的单端输入信号来说,其信号峰值应该 <=4Vpp(ADC的Vref=4.096),因为如果峰值达到了8Vpp,那么两支差分信号的峰值就会是4Vpp,两者相减,就不满足full-scale电压范围是[-Vref,+Vref],而变成[-2Vref,+2Vref]了,对吗?
5、我大概知道了THS431的Vcom脚的作用是为了抬高输出差分信号的共模电平,目的是使其差分信号都大于0。我还是想请教一下官方对Vcom的解释。