This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dac38j82 IOUTx 没有波形输出

Other Parts Discussed in Thread: DAC38J82, DAC38RF82

DAC使用DAC38J82,FPGA使用Xilinx XC7VX690T。 DAC设置为dual dac,LMFS配置的是8212,DAC与FPGA有8条LANE连接在一起 dacclk为1228.8Mhz,linerate为6144Mbps,dac和fpga的sysref为30.72Mhz,fpga的ref_clk和core_clk都是153.6Mhz。

FPGA可以选择频率控制字可设的DDS发出的正弦波,锯齿波和固定常数三种任意其一发送数据源。

FPGA和dac38j82之间jesd204b链路已经建立,一方面检测到了cgs和ilas过程,同时通过观察sync,该信号由低到高变化,之后一直为1即可得知链路已经建立。

fpga发送的数据通过gtN_txdata[31:0] gtN_txcharisk[3:0]底层数据端口也可以监测到;

读取DAC的config108寄存器,其bit 2 和bit 3 为0,没有报错,SERDES PLL锁定正常 。读取DAC的config100~config107寄存器,读回的值都是0x00000000,即fifo 正常,但 IOUTx 没有波形输出,有什么解决思路?谢谢

具体dac配置可以见附件,附件第一张图片device实际选的是dac38j82

 

dac38j82_software_setup.docx