This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ads1298工频干扰问题

Other Parts Discussed in Thread: ADS1298

请问ads1298怎么去除工频干扰,我测出的信号看起来很像50hz的工频干扰,请问这个干扰要用软件去除吗,还是在输入端搭电路或者是我测出的信号不对?

  • 这个50Hz是从电源上过来的?建议先检查一下50Hz工频干扰的来源,如果是从电源过来的,可以考虑优化一下电源,具体可以参考1298的EVM User Guide手册65页,EVM的信息在

    www.ti.com.cn/.../ads1298ecgfe-pdk

    另外,可否上传你的电路图,以及相关的测试图?看一下50Hz的干扰有多大。

  • 谢谢啊。电源就是你们官方给的,我用的3v的,工频干扰那个说起来比较乱,我先问这个吧,就是config2设置成0x10的时候,测试出来的测试信号的值比理论值要大很多,差不多是6——7倍,如果测试MVDD/4就直接超量程了。我设置成0xd0(把bit7,bit6设成1)的时候,测试出来是4/3倍,不知为何。我用的是内部参考源,2.4v。

  • 测试了一下发现电池供电不够。多谢。但是读出的测试信号仍然不正确,晶振没问题,SPI能够读出芯片号——0x92,应该是对的。然后就是发现,当我把SPI_START这个引脚置高时(芯片工作),即使我单步暂停下来,SPI_READY这个引脚会出现低电平脉冲,大约0.5s后又全变高,一直交替。程序使能START以后不运行就这样,不知为什么,我的采样率是500SPS.