您好,我在做AD转换的时候有两个问题:
有一个通道经过放大器输出后,有正确波形,但是用AD得到的数据却全是7FFFFF。我用的参考是2.4V内部,放大器输出为0.5-1.5V正弦波。
还有一个通道在AD工作的时候,放大器的输出会被拉低为0V左右。
除了这两个通道外,其余通道数据完全正常
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你的PGA增益打到哪个档位了?放大器单端输出还是差分输出?从手册上看,如果运放是单端输出,在应用时应该在另一个输入端加一个共模上去,比如你的放大器输出0.5~1.5V单端,那么另一个输入端应该给个1V的共模上去。如果运放是差分输出,那么根据手册第3页,AINP-AINN的范围应该是-VREF/Gain~+VREF/Gain。现在VREF=2.4V,如果要接收1.5V的信号,PGA Gain只能打到1,否则就会使输入超出允许范围。
对于运放输出拉低到0V的情况,怀疑可能是共模出了问题,最好上传一下电路图,以便进一步评估。
如果你的AINP是0.5V~1V,那么共模应该在1V,这种情况下建议你试试把AINN接一个1V共模电压,看看情况是否改善。
对于拉到0的通道,你可以把前端去掉,直接将信号输入到ADC的输入端,看看此时结果是否正确。如果结果正确,那说明问题出在前端,如果不正确,则调试ADC,使结果正确。