ADS8332技术参数里Offset error 最大为1mv,Vref为4.096V时1mV对应16个AD位。Gain error最大为0.25%FSR,对应163个AD位。对于精确测量来说这两个偏差能够引起很大的测量误差了。请问在使用过程中,需要补偿这两个误差么?应该如何减少这两个参数引起的测量误差!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
有些ADC集成了(ADS1256等)片上校准电路,可以通过寄存器配置来进行补偿,减小offset 和gain带来的error。
ADS8332没有集成self-calibration,但其实PCB 的GND处理,电源噪声,Vref的精度也都会引起ADC输出结果误差。 尽量从这些方面避免。