This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8688 八通道ADC转换的使用

Other Parts Discussed in Thread: ADS8688

大家好:

系统有8个传感器通道,参数如下:

信号范围: 0 ~ 10V

信号内阻:5K

信号带宽:1KHz

ADC采样精度分辨率:1mV

其它:传感器线缆较长(4M),现场伺服和电机等设备较多,有较大的共模干扰(线缆无屏蔽层)。

ADS8688 前端电路不知是否应该用仪表运放提高抗共模干扰能力,还是可以直接利用ADS8688的高输入阻抗和差分输入能力来实现ADC精度要求。

谢谢!

  • ADS8688这款AD的输入阻抗正好是高输入阻抗,优点就是避免再使用OP进行一个低阻抗的输出转换

    如果前端需要加仪表运放有效的提高CMRR,那么后端ADC的输入阻抗要低,换句话说,需要一个低输入阻抗源的ADC。